2015-08-27 03:05 AM
Hi all, I'm very new to this so please bear with me.
I'm using STM32L053 Nucleo and I set up normal polling USART to COM4 of the PC. I can send data to the serial monitor (PuTTy) but I can't receive anything back from PuTTy. When I try to type on PuTTy it doesn't seem to register anything, but since I can send I'm assuming that my USART is set up correctly..In my main: char *msg = ''Press a key.\n\r''; HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), 0xFFFF); HAL_UART_Receive(&huart2, (char*)c, strlen((char*)c), 0xFFFF); HAL_UART_Transmit(&huart2, (uint8_t*)endl, strlen(endl), 0xFFFF); msg = ''You pressed this key: ''; HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), 0xFFFF);The serial monitor prints out the following, and no matter what I press it makes no difference:>> Press a key.>> You pressed this key:This is how I intialised USART: /* USART2 init function */ void MX_USART2_UART_Init(void) { huart2.Instance = USART2; huart2.Init.BaudRate = 9600; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; huart2.Init.OneBitSampling = UART_ONEBIT_SAMPLING_DISABLED; huart2.AdvancedInit.AdvFeatureInit = UART_ADVFEATURE_NO_INIT; HAL_UART_Init(&huart2); } /* Initialise USART MSP */ void HAL_UART_MspInit(UART_HandleTypeDef* huart) { GPIO_InitTypeDef GPIO_InitStruct; if(huart->Instance==USART2) { /* Peripheral clock enable */ __USART2_CLK_ENABLE(); /**USART2 GPIO Configuration PA2 ------> USART2_TX PA3 ------> USART2_RX */ GPIO_InitStruct.Pin = GPIO_PIN_2|GPIO_PIN_3; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Pull = GPIO_PULLUP; GPIO_InitStruct.Speed = GPIO_SPEED_HIGH; GPIO_InitStruct.Alternate = GPIO_AF4_USART2; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); } }At this point I'm not sure if it's the code, the PuTTy setting, or the hardware. Any suggestion is appreciated. Thanks! #usart #stm32 #stm32l0532015-08-27 06:32 AM
I believe your problem is that you have set up a receive without knowing when a byte has been received from puTTy. What is needed is either a receive interrupt handler, or polling looking for a received byte.
Since you seem to be attempting polling, I recommend adapting the ''UART/UART_TwoBoards_ComPolling'' example project in the STM32L0 HAL Library. Edit: How are you assembling the input ''c'' into a transmit message buffer ? Cheers, Hal2015-08-27 07:10 AM
Hi,
Thank you so much for pointing me in the right direction!Added the code below and it works now. Thanks! 🙂if(HAL_UART_Receive(&huart2, (uint8_t *)aRxBuffer, RXBUFFERSIZE, 0xFFFF) != HAL_OK) { Error_Handler(); }