cancel
Showing results for 
Search instead for 
Did you mean: 

Checksum Error after download Firmware PackageSTM32F4 1.8.0

owl_bo
Associate
Posted on September 01, 2015 at 12:39

after download the Firmaware Package STM32F4 1.8.0 with STM32CubeMX Version 4.10.0, an error occurs: stm32cube_fw_f4_v180.zip (MD5 file checksum is not good).

It tried it several times on different PC's with the same errror.

Christian
4 REPLIES 4
ingwmeier
Senior
Posted on September 01, 2015 at 14:56

I had the same problem. Download through webpage, then extract 1.8 into repository directory works.

Posted on September 01, 2015 at 18:45

Hi Werner Meier,

After Upgrading STM32CubeMx to version 4.10.0, run it as Administrator (right click)  and download Firmware Package STM32F4 1.8.0.

-Shahrzad-
stephan2
Associate II
Posted on September 14, 2015 at 12:40

I tired running as administrator but still no luck. Why would you  make this such a pain. There is not even a link for manual loading. The webpage search did not bring up anything.... Aaaarg!

ingwmeier
Senior
Posted on September 14, 2015 at 17:06

http://www.st.com/web/catalog/tools/FM147/CL1794/SC961/SS1743/LN1897/PF259243#

 or manually select F4 Family then Resources Software STM32cube(1) there at the bottom you find it.