cancel
Showing results for 
Search instead for 
Did you mean: 

Motor Profiler for STEVAL-IHM023V3

KF Lam
Associate II
Posted on September 05, 2015 at 16:26

Hi,

We are using the STEVAL-IHM023V3 with the STM32VLDiscovery board for testing and we are able to run the motor without any problem. However, when we start to evaluate if we can use the STEVAL-IHM023V3 with a STM32F3xx board for testing the Motor Profiler feature, we found that the STMCWB doesn't support this. The STMCWB supports Motor Profiler for MB459, STEVAL-IHM028V2 and STEVAL-IHM025V1 only. Then we have studied the schematics of the IHM028V2 and IHM025V1 and compare these with the schematics of the IHM023V3. We cannot find any reason why STMCWB does not support Motor Profiler for IHM023V3. May I know that is there a way we can use IHM023V3 for Motor Profiler?

#motor-profiler #steval-ihm023v3
5 REPLIES 5
Gigi
Senior
Posted on September 07, 2015 at 14:32

Ciao

I think that this can be done with a workaround, starting a new project with STEVAL-IHM025V1 (that is very similar to the STEVAL-IHM023V3) and modify manually the power stage according the setting of STEVAL-IHM023V3.

You can open two instance of STM32 Motor Control Workbench one with the STEVAL-IHM023V3 and the other with a new project based on STEVAL-IHM025V1 go in the power stage and copy each value from one to the other project.

Ciao

Gigi

KF Lam
Associate II
Posted on September 07, 2015 at 14:58

Hi Gigi,

Thank you. I'll try this.

rsatterlee
Associate II
Posted on November 16, 2015 at 18:59

Could a similar thing be done for the STEVAL-IHM039V1? It is using a supported processor, but isn't listed as compatible with the Motor Profile in the SDK.

Gigi
Senior
Posted on January 07, 2016 at 18:13

Yes, I think shall work.

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards