cancel
Showing results for 
Search instead for 
Did you mean: 

Can't run RAW TCP server application in STM32f746disco

carlosmarcos
Associate II
Posted on September 19, 2016 at 20:48

I am trying to run a RAW TCP server app in the STM32F746disco. I have as starting point the F756 example. I have created the project with CubeMX and using Keil5.

I can't connect with my computer. I am debugging having several break points at callback functions, but the debug program doesn't stop at any of them (tcp_server_poll() or tcp_server_accept()). shouln't it do it? 

I don't have other idea to find out the problem.

Pins and configurations really seem OK since I 've got the examples.

Even Waveshare has an example exactly the same than the St examples.

Any help??

Thanks in advance.
2 REPLIES 2
Posted on September 19, 2016 at 21:19

I can't connect with my computer.

Via a cross-over cable, or through a hub/switch? Using Fixed IP addresses, or DHCP?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
carlosmarcos
Associate II
Posted on September 19, 2016 at 22:04

Hi!thanks for your reply. I had had to provide more info!

I just solved it. The problem with every example out there is that PHY ADDRESS is set to 1, and should be 0. Many days to find it out ;(