cancel
Showing results for 
Search instead for 
Did you mean: 

Keil5 project problem with CUBEMX4.16

carlosmarcos
Associate II
Posted on September 09, 2016 at 12:59

Hi,

I have updated CUBEMX version from 4.12 to 4.16. I create the MDK5 project using CubeMX...then I open it and it works. But when I attempt to manage Project items, I can't create a new GROUP (folder), Keil% doen't response and it gets stuck. 

It was working flawless until I updated the CubeMX version this morning.

Did it happen to anyone else, need to solve it??it is disgusting.

Also, is it possible to downgrade to 4.12 for example (was my previous installation)?

Thanks in advance.

Regards

Carlos

2 REPLIES 2
slimen
Senior
Posted on September 09, 2016 at 15:44

Hi,

I checked this case and I have same issue using CubeMx 4.16.1 !

It's not possible to downgrade previous version.

Regards

christoph2399
Associate II
Posted on September 13, 2016 at 08:20

i had the same problem, i cound not move around files in the project-window.

workaround:

  1. change in cubemx the project
  2. create a MDK-V4 projekt
  3. open it with  MDK V5
  4. you will be asked to MIGRATE the project
  5. click yes and save it as *uvprojx.

than you can ''manage'' your project