cancel
Showing results for 
Search instead for 
Did you mean: 

Request of STM32151RD USB_CDC Tutorial or Documentation.

avashalo
Associate II
Posted on October 05, 2015 at 06:37

Anyone implemented USB CDC on STM32L151? I am a beginner and working in a project which needs to implement PC to STM32L151RD USB communication. 

I have started with exploring STM32_USB_FS_4.0 examples. Can anyone suggest me any other related tutorials. I am using CoIDE 1.7.8 and not planning to use HAL libraries yet. 

Thanks in advance.
1 REPLY 1
Nesrine M_O
Lead II
Posted on October 06, 2015 at 17:30

Hi a.avash,

Have a look to the

http://www.st.com/web/en/catalog/tools/FM147/CL1794/SC961/SS1743/LN1734/PF258157?s_searchtype=keyword

 : it is a complete firmware and software package including examples and demos for all USB transfer types.

-Syrine-