cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DSL Min/Max specifications for ODR (Output Data Rate)

cn2
Associate II
Posted on March 21, 2017 at 15:35

I'm using the LSD6DSL in an application where the sampling rate (ODR for the MEMs) is important. The ODR in the datasheet is only given as 'Typical'. Could I get a more precise specification for the ODR, e.g. min/max values over the entire temperature range. I suppose this ODR is generated from an internal oscillator with tolerance, temperature drift, ...

1 REPLY 1
Miroslav BATEK
ST Employee
Posted on April 09, 2017 at 09:02

Unfortunately this information cannot be shared on ST Community web.