cancel
Showing results for 
Search instead for 
Did you mean: 

open an AC6 project

manuel239955_stm1_st
Associate II
Posted on November 09, 2015 at 16:23

Hello,

In a Cube project folder, when I click *.uvprojx, the project opens in Keil toolchain ; I build (0 error, 0 warning, great!!), and ready to run.

Likewise when I click *.eww and IAR toolchain.

What do I

click to open the project in AC6 ?

1 REPLY 1
Nesrine M_O
Lead II
Posted on November 09, 2015 at 17:32

Hi deschamps.manuel.001,

Yes, SW4STM32 is unlike Keil & IAR. 

To open an existing project with SW4STM32 you should follow this steps below:

• File >>Import

• Existing Projects into workspace (>>Next)

• Click on “Browse� for the root directory

• The projects list is refreshed (select then your project)  

• Ensure the option Copy projects into workspace is unchecked

• Then click Finish.

-Syrine –