2015-11-09 10:09 AM
Hi,
I'm trying to use multiple UARTs on the STM32F446 Nucleo board. I used STM32CubeMX to generate code that initializes all available UARTs and USARTs at 115200 baud and the MCU to run at 180MHz.void
my_putc(UART_HandleTypeDef* huart,
char
c) {
while
(!(huart->Instance->SR & USART_FLAG_TXE));
huart->Instance->DR = c;
}
void
my_puts(UART_HandleTypeDef* huart,
const
char
* s) {
while
(*s) {
my_putc(huart, *s);
++s;
}
}
int
main(
void
) {
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
MX_USART2_UART_Init();
MX_USART3_UART_Init();
MX_UART5_Init();
MX_UART4_Init();
MX_USART6_UART_Init();
/* USER CODE BEGIN WHILE */
while
(1) {
my_puts(&huart1,
''Hello UART1\n''
);
my_puts(&huart2,
''Hello UART2\n''
);
my_puts(&huart3,
''Hello UART3\n''
);
my_puts(&huart4,
''Hello UART4\n''
);
my_puts(&huart5,
''Hello UART5\n''
);
my_puts(&huart6,
''Hello UART6\n''
);
}
}
void
SystemClock_Config(
void
) {
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 8;
RCC_OscInitStruct.PLL.PLLN = 180;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
RCC_OscInitStruct.PLL.PLLQ = 2;
RCC_OscInitStruct.PLL.PLLR = 2;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
HAL_PWREx_ActivateOverDrive();
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK | RCC_CLOCKTYPE_PCLK1 | RCC_CLOCKTYPE_PCLK2;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_3);
}
However I only receive output on UART2 and UART3, all other UARTs are silent.
When connecting a scope it turns out that the other UARTs are much faster (the yellow line is UART6, the blue line UART3).
Why is that? What can I do to make them usable? They are all initialized in the same way (see usart.c).
#stm32f446 #hal #uart
2015-11-09 10:24 AM
It works when I use
RCC_OscInitStruct.PLL.PLLN = 160;
instead of
RCC_OscInitStruct.PLL.PLLN = 180;
Does that mean the MCU will only run at 160MHz?
2015-11-09 01:21 PM