cancel
Showing results for 
Search instead for 
Did you mean: 

FOC Library v4.3 available???

peterpeter9162
Associate II
Posted on October 03, 2016 at 17:37

I see in RN0085 that the FOC libary v4.3 is listed.  In new features for v4.3 I see AC6 workspace.  Yay! this is great for us.  We want to use the STM32 Open Development Env. as a base for all our firmware. 

Please can you give details on when will v4.3 be released?

Chris

#foc-4.3 #stm32-ode
3 REPLIES 3
Gigi
Senior
Posted on October 11, 2016 at 09:08

Ciao the new version is not released yet, we are still in qualification phase.

In few week probably we will have it published.

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards