cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F405 with 2 Shunts and FOC SDK

s61331
Associate II
Posted on December 02, 2015 at 14:05

Hello,

i want to generate a project with the WB for an existing hardware. But i can't configure the Ports for the 2 Analog Inputs of the Shunts.

Can you help me to configure the project?

Hardware:

STM32F405

Gate Driver DRV8302 with Amplifiers for two Shunts (1mOhm)
2 REPLIES 2
Gigi
Senior
Posted on January 07, 2016 at 17:58

Ciao Eric

You can select in the ST MC Workbench the two insulated current sensing as Current Sensing Network into the Power Stage section, then you have to select the two ADC input in the Control Stage -> Analog Input section.

Ciao

Gigi

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards