cancel
Showing results for 
Search instead for 
Did you mean: 

Cube Mx 4.22.0 don't generate CDC and Core files for the L475VGT

Roger Heil
Associate II
Posted on August 01, 2017 at 07:37

Hi,

the Cube MX Version 4.22.0 don't generate the Middleware/ST correct. The folder tree is correct, but not filled with files.

I tested with the L475VGT and add the Virtual Com Port.

#middleware #cube-mx #usb-cdc #4.22.0
1 ACCEPTED SOLUTION

Accepted Solutions
Imen.D
ST Employee
Posted on August 01, 2017 at 15:01

Hello

Heil.R

,

There is an issue with STM32CubeMX v4.22to merge the patch STM32CubeL4 v1.8.1 with existing STM32CubeL4 v1.8.0 source tree.

This issue isalready raised internally.

Try todelete existing STM32CubeL4 v1.8.0 firmware package and re-download/install the patch v1.8.1.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

View solution in original post

6 REPLIES 6
Posted on August 01, 2017 at 08:01

Hello!

In my PC generates all files correct

0690X00000603zQQAQ.jpg

Maybe you don't have full administrator rights to copy files to your folder.

0690X00000607mpQAA.png

Posible oolutions.

1. Add middleware as reference only.

2. Try to change the project folder name or/and path, and to take the proper rights to create files inside this folder.

Imen.D
ST Employee
Posted on August 01, 2017 at 11:30

Hello

Heil.R

,

Which firmware package version are you using ?

Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on August 01, 2017 at 11:59

L4 1.8.1

Posted on August 01, 2017 at 12:01

I got full admin rights. and the 'ref' files don't fit it. :|

Imen.D
ST Employee
Posted on August 01, 2017 at 15:01

Hello

Heil.R

,

There is an issue with STM32CubeMX v4.22to merge the patch STM32CubeL4 v1.8.1 with existing STM32CubeL4 v1.8.0 source tree.

This issue isalready raised internally.

Try todelete existing STM32CubeL4 v1.8.0 firmware package and re-download/install the patch v1.8.1.

Best Regards

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Posted on August 01, 2017 at 13:54

Is it possible to get a older version of cube mx?