cancel
Showing results for 
Search instead for 
Did you mean: 

STMStudio Installation and Launch

k239955_stm1
Associate
Posted on January 31, 2016 at 12:37

Hello,

I have recently installed STMStudio on my computer. The problem is that I can't launch the program. My operating system is Windows 8.1, I have installed Java JDK and JRE 8u71 in both 32bit and 64bit versions. Then I installed STMStudio v3.4. There is a .jar file that is supposed to be oppened by javaw aplication but it doesn't. I've tried many different ways to launch it: by shortcut, by .jar file, by command line. Up to this momment nothing works.

Help, please.

#stm-studio-installation-java-jre
1 REPLY 1
S C
ST Employee
Posted on February 01, 2016 at 11:23

Hello,

There is an issue with STMStudio-3.4 and JRE1.8: the shortcuts are wrongly computed by the installation setup. The path to javaw.exe is wrong. It has to be manually modified in order to point to javaw.exe of the 32-bits version of JRE. Do not modify the other parameters of the shortcut.

A version 3.5 of the STMStudio is about to be delivered fixing this issue