2015-12-17 01:40 AM
According to the
(CMSIS version 1.02) the return value should be the number of tokens available. This is a citation from the documentation: ''The return value indicates the number of available tokens (the semaphore count value). If 0 is returned, then no semaphore was available.'' However, the implementation in STM32CubeF7 returns osOK (which is 0) when the semaphore is acquired. Is this the intended behaviour? Is the documentation wrong? The implementation in STMCubeF7looks like this:int32_t osSemaphoreWait (osSemaphoreId semaphore_id, uint32_t millisec)
{
TickType_t ticks;
portBASE_TYPE taskWoken = pdFALSE;
if (semaphore_id == NULL) {
return osErrorParameter;
}
ticks = 0;
if (millisec == osWaitForever) {
ticks = portMAX_DELAY;
}
else if (millisec != 0) {
ticks = millisec / portTICK_PERIOD_MS;
if (ticks == 0) {
ticks = 1;
}
}
if (inHandlerMode()) {
if (xSemaphoreTakeFromISR(semaphore_id, &taskWoken) != pdTRUE) {
return osErrorOS;
}
portEND_SWITCHING_ISR(taskWoken);
}
else if (xSemaphoreTake(semaphore_id, ticks) != pdTRUE) {
return osErrorOS;
}
return osOK;
}
2015-12-23 07:54 AM
Hi gjesse.soren,
This incoherence is already detected and reported ([DEAD LINK /public/STe2ecommunities/mcu/Lists/STM32Java/Flat.aspx?RootFolder=/public/STe2ecommunities/mcu/Lists/STM32Java/Bug%20in%20CMSIS_OS%20for%20FreeRTOS%20V1.02&¤tviews=101]Bug in CMSIS_OS for FreeRTOS V1.02.Thank you for your feedback.-Shahrzad-2017-09-05 01:09 PM
Found this bug too. Happy it was reported. Having to figure out how many tokens I have is a pain otherwise.