cancel
Showing results for 
Search instead for 
Did you mean: 

VCP driver issue for Windows 7. can recognize in Windows 10

rumlyen
Associate II
Posted on September 16, 2016 at 23:29

Hello all.

Windows 10 can well recognize my STM32L1 device (custom PCB) as 'USB Serial device' but same isn't recognizing in Windows 7 (another PC). I've tried both VCP driver 1.3 and 1.4 in windows 7. Do I need to change any configuration anywhere to make it run in Windows 7. I've used USB_FS_4.0 library in this project.

I appreciate your comments here.
1 REPLY 1
slimen
Senior
Posted on September 29, 2016 at 16:24

Hello,

Do you get an error message ?

If you can test and check this issue with another Pc (Windows 7), in order to deduce if the problem here seems related to the hardware or software environment.

Regards