cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F303 Eval Board CAN Normal Mode

akshayamk
Associate II
Posted on December 22, 2015 at 02:06

Hello!

Referring to the CAN Networking sample codes in Cube MX F3 package, I tried it out by connecting 2 STM32F303 Eval Boards. I used a female-female connector to connect the two boards. However, I am not able to transmit as on debug mode, the codes are getting stuck at HAL_CAN_Transmit(&CanHandle, 10).

Then, I referred to CAN Networking sample codes from Standard peripherals library and when I ran the programme, it worked as mentioned in readme text file. That is, when I pressed the KEY button, the LED changed from LED1 to LED2 to LED3 and so on. However, when I try to transmit a CAN frame by pressing on th KEY button on one board, the other board is not receiving as I am unable to hit receive handler on the codes.

Do I need to have additional jumper settings for my set-up? Any help is appreciated! Thank you!
0 REPLIES 0