cancel
Showing results for 
Search instead for 
Did you mean: 

Which is the best Stereo Audio SAI or I2S solution ?

T J
Lead
Posted on February 15, 2017 at 21:38

I can use one SAI RxTx channel  or Two separate SAI ports,  providing independent Rx and Tx channels.

Which solution supplies the best HD stereo audio quality ? (stereo and bass channel would be great)

The Speaker drive can be separated from the Audio codec but I am all ears on any suggestions.

My processor board is based on the STM32F7 series processors I am developing my own low level drive software, to facilitate a smaller code footprint and the highest quality seamless Stereo Audio I/O.

The design is working toward a Skype/Gypsy Audio interface, and to reproduce reasonable quality music.

Which software protocol is better ?  SAI,  I2S, PCM , SPDIF ?

I see the SAI port has an 8 byte fifo shared between Rx and TX channels. how can that be full duplex ?

which Codec can someone suggest ?  for High quality Stereo..

do we need a separate drive ? 10W is huge for this...

#audio-drive #audio-codec
0 REPLIES 0