cancel
Showing results for 
Search instead for 
Did you mean: 

TIMER Question

mbmail4
Associate II
Posted on January 13, 2016 at 04:53

Hi Everyone.

I've looked through some of the older posts re: timer delay function, and I have used one of those posts as a base to what I have implemented. The problem is, when I run the delay function in a loop to test, it runs for about one second then it stops (crashes?).

From what I've read so far, my set up should be a free running 16bit counter.

Can anyone see what the problem is.

      TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

      RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

      TIM_TimeBaseStructure.TIM_Prescaler = 0x0;

      TIM_TimeBaseStructure.TIM_Period = 0xFFFF;

      TIM_TimeBaseStructure.TIM_ClockDivision = 0x0;

      TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

      TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

      TIM_Cmd(TIM2, ENABLE);

   while(1)

   {

   GPIOC->BRR  = GPIO_Pin_11;

   delay(100);

   GPIOC->BSRR = GPIO_Pin_11;

   delay(100);

   }

     

void delay(uint16_t ticks)

{

  uint16_t start = TIM2->CNT;

  do { } while((TIM2->CNT - start) < ticks);

}
7 REPLIES 7
Radosław
Senior
Posted on January 13, 2016 at 10:25

  do { } while((uint16_t)(TIM2->CNT - start) < ticks);

Posted on January 13, 2016 at 12:43

Stops where? Use a debugger.

Is this an F1 part? What specific STM32

If an F2/F4 TIM2 is 32-bit, suggest you configure it as such, and use uint32_t, it will be more efficient that 16-bit, and won't potentially need casting

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
pkumar1883
Associate II
Posted on January 13, 2016 at 14:48

Hi b.m.002,

If you only want to make a timer based delay function then I would recommend to use

systick.

It uses very less configurations. Easy to use.

If need help for TIMER problem then mention your STM32 part number. So that specific help can be provided.

Walid FTITI_O
Senior II
Posted on January 13, 2016 at 16:37

Hi b.m.002,

You have to enable the Timer counter the moment of start ( begin of delay function), and not before.

-Hannibal-

mbmail4
Associate II
Posted on January 14, 2016 at 00:34

Thanks everyone for your input. I have a STM32VLDISCOVERY fitted with the STM32F100RBT6B microcontroller.

I've made some changes, and what I want to do is have a delay routine available that will give me 1uS granularity. Generally most applications need delays in the low mS, but for this exercise I want to figure out why this setup is not working.

When I changed the location the timer was enabled, this worked for the previous setup, but it counted some other delay value which for testing at the time was not important. The code below is hopefully set up to produce 1uS events, and this does not seem to work at the moment, the timer does not seem to want to start at all, maybe its something I don't understand about the way timers work in the stm32? If I got it correct, then TIMER2 roll over should occur at 1/24Mhz * 65535 = 2.7mS, so in the main loop delaying for 100 should work ie: 100uS.

void TIMER2_Configuration_new(void)

{

  TIM_TimeBaseInitTypeDef TIM_TimeBaseStructure;

  RCC_APB1PeriphClockCmd(RCC_APB1Periph_TIM2, ENABLE);

  TIM_TimeBaseStructure.TIM_Prescaler = 23;

  TIM_TimeBaseStructure.TIM_Period = 0;

  TIM_TimeBaseStructure.TIM_ClockDivision = 0x0;

  TIM_TimeBaseStructure.TIM_CounterMode = TIM_CounterMode_Up;

  TIM_TimeBaseInit(TIM2, &TIM_TimeBaseStructure);

}

void delay(uint16_t ticks)

{

  TIM_Cmd(TIM2, ENABLE);

  uint16_t start = TIM2->CNT;

  do { } while((TIM2->CNT - start) < ticks);

  TIM_Cmd(TIM2,DISABLE);

}

Thanks

Martin.
Posted on January 14, 2016 at 03:45

TIM_TimeBaseStructure.TIM_Period = 0; // No going to work

TIM_TimeBaseStructure.TIM_Period = 0xFFFF; // Maximal 0..65535

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
mbmail4
Associate II
Posted on January 14, 2016 at 04:36

Hi clive, I change the period setting to 0xFFFF, but its still wont work? so far I haven't figured out what else to try. It works briefly and then stops.

My scope trace seems to show the period to be correct for the setup, that is, its a 100uS dely.