cancel
Showing results for 
Search instead for 
Did you mean: 

STLINK and CPU reset.

mbmail4
Associate II
Posted on August 22, 2016 at 15:06

Hi.

Recently I noticed when reprogramming my stm32vl discovery board, STLINK does not reset the chip and start my newly programmed application. Its been such a long time since I did any work on this and I believe in the past it would reset the cpu after a re flash. Did I imagine this, or has something changed I did not notice. Has anyone else experienced this?

I’m using STLINK utility V3.8.0

Martin

2 REPLIES 2
Walid FTITI_O
Senior II
Posted on August 22, 2016 at 15:50

Hi b.m.002,

Check the SB11 solder bridge which should be ON. One more thing , the STM32VL DISCO does not need any ST-Link firmware installation, that is already embedded inside.

-Hannibal-

mbmail4
Associate II
Posted on August 27, 2016 at 04:26

Hi Hannibal, that was ok, but I have since connected my Nucleo, and I have notice even this board will not reset automatically after I reprogram the micro, I have to press the reset button for my app to start, any ideas.

thanks