2018-04-17 06:16 PM
Hi, I am trying to set up an STM32f030 to do ADC conversions on 4 channels using interrupts and no DMA. The first ADC input gets good values but the second ADC inf put is wonky.I used CubeMX to generate the code. I am a noob and wish to get the ADC working before diving into DMA. Any help would be appreciated.#
Here is the code:
void HAL_ADC_ConvCpltCallback(ADC_HandleTypeDef* AdcHandle)
{ switch(CurChannel) { case 0: Adc_Raw_X = HAL_ADC_GetValue(AdcHandle); CurChannel++; AvgAdc[0]+=Adc_Raw_X; cntAvgAdc[0]+=1; if(cntAvgAdc[0]>=16) { cntAvgAdc[0] = 0; AvgAdc[0] = AvgAdc[0] / 16; flgInputChanged=1; } break; case 1: Adc_Raw_Y = HAL_ADC_GetValue(AdcHandle); CurChannel++; AvgAdc[1]+=Adc_Raw_Y; cntAvgAdc[1]+=1; if(cntAvgAdc[1]>=16) { cntAvgAdc[1] = 0; AvgAdc[1] = AvgAdc[1] / 16; flgInputChanged=1; } break; case 2: Adc_Spare1 = HAL_ADC_GetValue(AdcHandle); CurChannel++; break; case 3: Adc_Spare2 = HAL_ADC_GetValue(AdcHandle); CurChannel++; HAL_ADC_Stop_IT(&hadc); break; }}static void MX_ADC_Init(void)
{ADC_ChannelConfTypeDef sConfig;
/**Configure the global features of the ADC (Clock, Resolution, Data Alignment and number of conversion)
*/ hadc.Instance = ADC1; hadc.Init.ClockPrescaler = ADC_CLOCK_ASYNC_DIV1; hadc.Init.Resolution = ADC_RESOLUTION_12B; hadc.Init.DataAlign = ADC_DATAALIGN_RIGHT; hadc.Init.ScanConvMode = ADC_SCAN_DIRECTION_FORWARD; hadc.Init.EOCSelection = ADC_EOC_SINGLE_CONV; //hadc.Init.EOCSelection = ADC_EOC_SINGLE_SEQ_CONV; hadc.Init.LowPowerAutoWait = DISABLE; hadc.Init.LowPowerAutoPowerOff = DISABLE; hadc.Init.ContinuousConvMode = ENABLE; hadc.Init.DiscontinuousConvMode = DISABLE; hadc.Init.ExternalTrigConvEdge = ADC_EXTERNALTRIGCONVEDGE_NONE; hadc.Init.DMAContinuousRequests = DISABLE; hadc.Init.Overrun = ADC_OVR_DATA_PRESERVED; if (HAL_ADC_Init(&hadc) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_1; sConfig.Rank = ADC_RANK_CHANNEL_NUMBER; sConfig.SamplingTime = ADC_SAMPLETIME_239CYCLES_5; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/sConfig.Channel = ADC_CHANNEL_1;
if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_2; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }/**Configure for the selected ADC regular channel to be converted.
*/ sConfig.Channel = ADC_CHANNEL_3; if (HAL_ADC_ConfigChannel(&hadc, &sConfig) != HAL_OK) { Error_Handler(); }}2018-04-17 06:20 PM