cancel
Showing results for 
Search instead for 
Did you mean: 

attach only stm8

manuel239955_st
Associate
Posted on January 08, 2016 at 14:06

is it possible with the stvd to attach / connect only to a already running target via swim?

#swim #stm8 #attach
1 REPLY 1
Philipp Krause
Senior II
Posted on January 13, 2016 at 13:13

I'm not using STVD, but in general, STVD is more complete than the free tools. With the free stm8flash, I can attach to a running target to write a new program into the flash memory via ST-Link or ST-Link/v2 anytime. So I guess it will work fine with STVD.

Philipp