cancel
Showing results for 
Search instead for 
Did you mean: 

Compability issues with UDE

simone
Associate II
Posted on January 22, 2016 at 16:17

I'm using the MPC5643L from nxp on the modular+minimodule board. Do you know if it is possible to program it with  http://www.st.com/web/en/catalog/tools/PF258744  using the UDE debugger? I apparently can connect but I can't debug and I don't know if it is possible or not.

Thank you very much.

1 REPLY 1
Erwan YVIN
ST Employee
Posted on January 25, 2016 at 11:34

Hello Simon ,

I think that it should work ...(same device)

Maybe you need to create a new workspace with Freescale reference with PLS to take the hand.

(cf screenshot)

Could you give your minimodule reference ?

Could you check if PLS FTDI A/B are available in your Windows (Device Manager) after switch-on the board ?

Best regards

Erwan

________________

Attachments :

2016-01-25_113129.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qVW6&d=%2Fa%2F0X0000000bnx%2FBaYroynXZgMeZ1iv_ZsOQ3QrbLlXHJb3DU_7mmGguM8&asPdf=false