2016-11-04 08:49 PM
Hi
I have been using my F3discovery to build an application, which is now finished, so I designed a new user PCB and after assembling and running my application all went well, until I tried to start the debugger with mu new PCB.
I get the following error:
Error in final launch sequence
Failed to execute MI command: load D:\\emb\\ARM\\ST\\SW4STM32\\F3\\work\\DAQ\\DAQv2\\Debug\\DAQv2.elfError message from debugger back end:
Error erasing flash with vFlashErase packet Error erasing flash with vFlashErase packetI think its because ST-LINK utility is trying to use the F3discovery config file to start the debugger.
Can someone help me understand how to create a custom config file.
I'm using ST-LINK /V2 ICD tool. I have 5 JTAG connections on my board:
TMS, TCK, TDO, TDI, NRST.
Thanks
kvresto
2016-11-04 09:42 PM
Also why is it when I debug the F3discovery board, the debugger jumps around all over the place, and I cant tell which instruction I'm executing. I have not programed for any timer interrupts.
thanks
2016-11-04 11:43 PM
..the debugger jumps around all over the place..
Turn off optimization, there is frequently not a one-to-one relationship between C source lines, and the assembler code, and the optimizer can change the linear flow.
2016-11-06 01:44 PM
Thanks Clive, now I can step through the code.
I noticed you have changed your profile, what revolution are you referring to?
kvresto
2016-11-06 03:49 PM
I'm expecting one to start on November 8th.... but I perceive there are larger things afoot...
2016-11-06 04:00 PM
Viva la revolución (i think) 🙂