2018-05-10 10:06 AM
Hello, I have a board with stm32f446rc processor and I don't get to connect bootloader with stm32 flashloader.
Following below this function used to access the bootloader on chip. I am using USART1 (PA9,PA10) to connect RS232.
void JumpToBootloader(void) {
void (*SysMemBootJump)(void);/**
* Step: Set system memory address. * * For STM32F446, system memory is on 0x1FFF 0000 * For other families, check AN2606 document table 110 with descriptions of memory addresses */ volatile uint32_t addr = 0x1FFF0000;/**
* Step: Disable RCC, set it to default (after reset) settings * Internal clock, no PLL, etc. */ RCC_DeInit(); __HAL_RCC_SYSCFG_CLK_ENABLE(); /** * Step: Disable systick timer and reset it to default values */ SysTick->CTRL = 0; SysTick->LOAD = 0; SysTick->VAL = 0; /** * Step: Disable all interrupts */ __disable_irq();__DSB();
/**
* Step: Remap system memory to address 0x0000 0000 in address space * For each family registers may be different. * Check reference manual for each family. * * For STM32F4xx, MEMRMP register in SYSCFG is used (bits[1:0]) * For STM32F0xx, CFGR1 register in SYSCFG is used (bits[1:0]) * For others, check family reference manual */ __HAL_SYSCFG_REMAPMEMORY_SYSTEMFLASH(); //Call HAL macro to do this for you/**
* Step: Set jump memory location for system memory * Use address with 4 bytes offset which specifies jump location where program starts */ /* Remap is bot visible at once. Execute some unrelated command! */ __DSB(); __ISB();SysMemBootJump = (void (*)(void)) (*((uint32_t *)(addr + 4)));
/** * Step: Set main stack pointer. * This step must be done last otherwise local variables in this function * don't have proper value since stack pointer is located on different position * * Set direct address location which specifies stack pointer in SRAM location */ __set_MSP(*(uint32_t *)addr);/**
* Step: Actually call our function to jump to set location * This will start system memory execution */SysMemBootJump();
/**
* Step: Connect USB<->UART converter to dedicated USART pins and test * and test with bootloader works with STM32 Flash Loader Demonstrator software */while(1);
}2018-05-10 10:12 AM
2018-05-11 07:01 AM
>
volatile uint32_t addr = 0x1FFF0000;
You've forgotten to set bit 0 in the jump address. It is required for the thumb instruction set.
- pa
2018-05-11 08:12 AM
Thank you Clive,
so I tried to put in bootloader mode with BOOT0=HIGH, but it didn't work communication between board and stm32 loader.
I don't know what is happening.
2018-05-11 08:40 AM
The loader is going to be highly sensitive to transitions on any of the pins/interfaces where valid activity might be expected. This might take precedence over your signalling on PA9/PA10 later.
Review board design and pin usage.
2018-05-11 09:03 AM
>>You've forgotten to set bit 0 in the jump address. It is required for the thumb instruction set.
Yeah, that's not how it works in this context, it is a table full of addresses, not the address it is calling. The address of the ROM Vector Table is correct.