cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429I DISCO Win 8 Driver

ejanuska
Associate II
Posted on February 04, 2016 at 04:54

I regretfully bought a STM32F429I DISCO board and I plugged it in to my Win 8 PC. I was hoping to use this platform with mbed. Well the board is supposed to show up as a usb device but it doesn't.

I installed the drivers and updated the firmware, installed ST LINK. Uninstalled the drivers and reinstalled them. Reboot, reset, etc.

Wasting a ton of my time just trying to figure out how mbed is going to work with this board and my PC.

I don't even want to install an IDE to find out it still isn't going to work because of drivers or something else.

So dissapointed.

#fail #notworking #rtfm-lmgtfy #poordrivers
1 REPLY 1
Posted on February 04, 2016 at 12:36

If you updated the firmware, then clearly the drivers are working.

Does this board support mbed drag-n-drop, don't seem to recall it being one that did, that would be the NUCLEO boards, and the newer DISCO (F469 and F746) boards.

http://www.st.com/web/catalog/tools/FM116/CL1620/SC959/SS1532/LN1848/PF262395?icmp=tt2951_gl_pron_oct2015&sc=stm32f469idiscovery

https://developer.mbed.org/platforms/ST-Discovery-F469NI/

https://developer.mbed.org/platforms/ST-Discovery-F429ZI/

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..