cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F429 LTDC @ 1280x720 resolution

Posted on May 22, 2017 at 16:17

Hello everyone,

I already successfully used the LTDC to create a VGA Signal with a Resolution of 800x480 Pixel with 16bit

colour with decent performance. All configuration was done with CubeMX for the LTDC.

AN4861 claims that the STM32F429 can support a resolution of 1280x720 Pixel. But this Resolution is not

possible with CubeMX, because the visible horizontal Resolution is limited to 1024 Pixel. After a quick check in the datasheet, the Register for the horizontal Resolution is limited to 2048 Pixel. Is there a Special reason for this Limitation in CubeMX ?

Am I forced to configure the LTDC manually for this Resolution or will there be a fix for CubeMX ?

Best regards,

Markus.

PS: I would like to see some example Code for the STM32F769I-DISC1 with the B-LCDAD-HDMI1 Adapter with this Resolution.

1 REPLY 1
Posted on July 21, 2017 at 20:44

OK, problem solved with CubeMX 4.22.

A little test project shows the capabilities of the STM32F429i-Disco with an external monitor.

https://youtu.be/miGGfDeDFWU

 

The next step will be the STM32F769I-DISC1 with the B-LCDAD-HDMI1 Adapter.

Any advice how to use the DSI/HDMI interface ?

Best regards,

Markus Horbach.