cancel
Showing results for 
Search instead for 
Did you mean: 

how to use BSP in general / IHM01A1

Posted on May 18, 2016 at 16:05

Hello everybody,

I am experimenting with an Nucleo-STMF030R8 and the X-Nucleo-IHM01A1 Expansion board. The example Project from STM32CubeExpansion-SPN1_V1.6.0

is working fine and i also managed to modify this Project.

Now I want to use the BSP for my own Project and add some extra Hardware (ili9341 + Buttons + poti) as user Input to control the stepper Motor. I used the chapter SDRAM BSP from the ''STM32F4 Labs'' Document to get a clue how to use BSPs in general. But I am failing to add the BSP to my CubeMX generated Keil Project. The extra Hardware is working, but adding the BSP stalls the uC. Is there a special manual how to use BSPs in own Projects ?

Thanks in advance for some hints.
1 REPLY 1