cancel
Showing results for 
Search instead for 
Did you mean: 

STM32CubeMX v4.26.0 makefile code generation error

Innomatic
Associate II
Posted on June 17, 2018 at 04:38

Hi,

I think I encountered with code generation error of STM32CubeMX v4.26.0 in Makefile setting. This is how to regenerate it:

1. Create any project

2. Generate code with Makefile setting.

3. Close CubeMX

4. Find the project folder and open up CubeMX by double clicking on the ioc file.

5. Try to regenerate code.

Workaround is to delete Makefile (and Makefile_tmp if exists) before opening up the CubeMX. So it looks like CubeMX failed to overwrite existing Makefile.

Thanks,

2 REPLIES 2
Nawres GHARBI
ST Employee
Posted on June 27, 2018 at 16:09

Hi lee, 

This will be fixed soon in the 4.27.0

Tejas_Tj
Associate

I'm still facing that error in STM32CubeMX 4.27.0