cancel
Showing results for 
Search instead for 
Did you mean: 

LSM6DS3 Delay

Konami
Senior
Posted on April 19, 2017 at 23:28

I'm using the LSM6DS3 to control a gimbal with a camera on it, and I'm noticing that my control is suffering due to delay in the system. I have configured the LSM6DS3 for an output datarate of 208Hz, with the fifo in bypass mode and I'm also sampling the sensor at 208Hz. However when I measure the delta between a physical input to the camera and the observable difference in the LSM6DS3 readings, I see about 20ms of delay. When I increase the datarate of the sensor to 833Hz, the delay is reduced to roughly 10ms, but this delay still seems rather large.

Is there any spec on the bandwidth/ delay/ latency of this sensor? What can I do to get the absolute latest readings from it?

#lsm6ds3
0 REPLIES 0