cancel
Showing results for 
Search instead for 
Did you mean: 

STM32f429 USB OTG problem

radupaulstefan
Associate II
Posted on March 07, 2016 at 18:23

Hello everyone,

I tried to import an usb library in Atollic TrueStudio . I receive this error 

''fatal error: usbd_msc_mem.h: No such file or directory''.In fact that is such ''file or directory'' included in my project as the picture show.

0690X000006037iQAA.jpg

Can you help me solve this problem ?

Thank you.
1 REPLY 1
slimen
Senior
Posted on March 08, 2016 at 17:11

Hello radu.paul,

Could you please provide more details about the source of the example you are using. 

I suggest you to try this example that you can find in the STM32CubeF4 package:

STM32Cube_FW_F4_V1.11.0\Projects\STM324x9I_EVAL\Applications\USB_Device\MSC_Standalone\TrueSTUDIO

-ForumSTM32-