cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f407 EXTI interruption freeze

karolalexandersecret
Associate II
Posted on March 01, 2016 at 12:11

Hi all,

Trying to implement a basic external interruption on the stm32f407 discovery board, the microcontroller allways freeze after receiving external interrupt. After some test i discover interrupt cause a call to the Hard Fault Interrupt and the CPU enter infinite loop. (The infinite loop is defined by default in the Startup ASM file)

The code is verified several time and i don't understand the problem. I add some code to verify that the CPU go into the Hard_Fault_Handler. Here it is:

#include ''stm32f4xx.h''

#include <stdint.h>

#include ''stm32f4xx_rcc.h''

GPIO_InitTypeDef g1,g2;

EXTI_InitTypeDef i;

NVIC_InitTypeDef nvic_i;

uint32_t j;

void On(void);

void delay(void);

void Off(void);

void delay2(void);

int main(void)

{

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOD, ENABLE);

RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOA, ENABLE);

RCC_APB2PeriphClockCmd(RCC_APB2Periph_SYSCFG, ENABLE);

g1.GPIO_Pin= GPIO_Pin_12;

g1.GPIO_Mode= GPIO_Mode_OUT;

g1.GPIO_OType=GPIO_OType_PP ;

g1.GPIO_PuPd= GPIO_PuPd_NOPULL;

g1.GPIO_Speed= GPIO_Speed_100MHz;

g2.GPIO_Pin=GPIO_Pin_0;

g2.GPIO_Mode= GPIO_Mode_IN;

g2.GPIO_OType=GPIO_OType_PP ;

g2.GPIO_PuPd= GPIO_PuPd_DOWN;

g2.GPIO_Speed= GPIO_Speed_2MHz;

GPIO_Init(GPIOD, &g1);

GPIO_Init(GPIOA, &g2);

SYSCFG_EXTILineConfig(EXTI_PortSourceGPIOA, EXTI_PinSource0);

i.EXTI_Line= EXTI_Line0;

i.EXTI_LineCmd= ENABLE;

i.EXTI_Mode= EXTI_Mode_Interrupt;

i.EXTI_Trigger= EXTI_Trigger_Rising;

EXTI_Init(&i);

nvic_i.NVIC_IRQChannel= EXTI0_IRQn;

nvic_i.NVIC_IRQChannelCmd= ENABLE;

nvic_i.NVIC_IRQChannelPreemptionPriority= 0x06;

nvic_i.NVIC_IRQChannelSubPriority= 0x06;

NVIC_Init(&nvic_i);

while(1){

On();

delay();

Off();

delay();

}

}

void On(){

GPIO_SetBits(GPIOD, GPIO_Pin_12);

}

void Off(){

GPIO_ResetBits(GPIOD, GPIO_Pin_12);

}

void delay(){

for(j=0;j<0xffffff;j++);

}

void delay2(){

for(j=0;j<0x0fffff;j++);

}

void EXTI0_IRQHandler(void){

// Make sure that interrupt flag is set

if (EXTI_GetITStatus(EXTI_Line0) != RESET) {

// Do your stuff when PA0 is changed

//pause();

GPIO_ToggleBits(GPIOD, GPIO_Pin_12);

// Clear interrupt flag

EXTI_ClearITPendingBit(EXTI_Line0);

}

}

void HardFault_Handler(void){

while(1){

On();

delay2();

Off();

delay2();

}

}

Does someone know what i do wrong ?

Alexander

4 REPLIES 4
Posted on March 01, 2016 at 17:40

What tool chain are you using?

What are the defines passed into the compiler?

Which startup file is being used?

You have reviewed this with a debugger?

C++ or .cpp?

I might do this differently, but the code doesn't look unreasonable.

Use local variables for the delay iterators, with a volatile definition.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
karolalexandersecret
Associate II
Posted on March 02, 2016 at 10:38

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6jR&d=%2Fa%2F0X0000000buA%2FHXK1Sz56uIRkb.4IbH6b5jkDyR5EYTvbhMzHvkomFWY&asPdf=false
Posted on March 02, 2016 at 20:33

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6jD&d=%2Fa%2F0X0000000bu3%2FsUwSX8VCsrFvDtVTnH_LqYjxulo2KAk6UQ9_za8kOBI&asPdf=false
Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
karolalexandersecret
Associate II
Posted on March 02, 2016 at 21:14

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6f1&d=%2Fa%2F0X0000000bsd%2FPdciVfuGZcl0C6SHqBIeaXrXm2kz6S0COY.8UacjV28&asPdf=false