2016-03-09 02:55 AM
Hi,
I have successfully configure CAN2 in STM32F429ZI discovery board. But when I am trying to transmit message it goes to transmit pending state. I have configure the baudrate of 500k at PCLK1 frequency 45MHz. I also share my code below. Please anyone help me to find problem.static void CAN_Config(void){ GPIO_InitTypeDef GPIO_InitStructureCAN_RX; GPIO_InitTypeDef GPIO_InitStructureCAN_TX; CAN_InitTypeDef CAN_InitStructure ; /* Enable the GPIO Clock */ RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN1, ENABLE); RCC_APB1PeriphClockCmd(RCC_APB1Periph_CAN2, ENABLE); //CAN2 Peripharal clock RCC_AHB1PeriphClockCmd(RCC_AHB1Periph_GPIOB, ENABLE); GPIO_PinAFConfig(CAN2_Port, GPIO_PinSource12, GPIO_AF_CAN2); //CAN_RX = PB12 GPIO_PinAFConfig(CAN2_Port, GPIO_PinSource13, GPIO_AF_CAN2); //CAN_TX = PB13 /* Configure the GPIO_CAN_Rx pin */ GPIO_InitStructureCAN_RX.GPIO_Pin = CAN2_Rx; GPIO_InitStructureCAN_RX.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructureCAN_TX.GPIO_OType = GPIO_OType_PP; GPIO_InitStructureCAN_TX.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_InitStructureCAN_RX.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(CAN2_Port, &GPIO_InitStructureCAN_RX); /* GPIO CAN_TX Configuration */ GPIO_InitStructureCAN_TX.GPIO_Pin = CAN2_Tx; GPIO_InitStructureCAN_TX.GPIO_Mode = GPIO_Mode_AF; GPIO_InitStructureCAN_TX.GPIO_OType = GPIO_OType_PP; GPIO_InitStructureCAN_TX.GPIO_PuPd = GPIO_PuPd_NOPULL; //GPIO_InitStructureCAN_TX.GPIO_PuPd = GPIO_PuPd_UP; GPIO_InitStructureCAN_TX.GPIO_Speed = GPIO_Speed_50MHz; GPIO_Init(CAN2_Port, &GPIO_InitStructureCAN_TX); CAN_DeInit(CAN2);//CAN_FilterConfiguration(); /* CAN2 configuration */ CAN_InitStructure.CAN_TTCM = DISABLE; // Time-triggered communication mode = DISABLED CAN_InitStructure.CAN_ABOM = DISABLE; // Automatic bus-off management mode = DISABLED CAN_InitStructure.CAN_AWUM = DISABLE; // Automatic wake-up mode = DISABLED CAN_InitStructure.CAN_NART = DISABLE; // Non-automatic retransmission mode = DISABLED CAN_InitStructure.CAN_RFLM = DISABLE; // Receive FIFO locked mode = DISABLED CAN_InitStructure.CAN_TXFP = DISABLE; // Transmit FIFO priority = DISABLED CAN_InitStructure.CAN_Mode = CAN_Mode_Normal; // Normal CAN mode //CAN_InitStructure.CAN_Mode = CAN_Mode_Silent; CAN_InitStructure.CAN_SJW = CAN_SJW_1tq; // Synchronization jump width = 1 CAN_InitStructure.CAN_BS1 = CAN_BS1_13tq; //14 CAN_InitStructure.CAN_BS2 = CAN_BS2_4tq; //6 CAN_InitStructure.CAN_Prescaler = 5; // Baudrate 500 kbps //CAN_InitStructure.CAN_Prescaler = 16; // Baudrate 125 kbps //x=CAN_Init( CAN2, &CAN_InitStructure); if(CAN_Init( CAN2, &CAN_InitStructure)) { /* Initialize LEDs mounted on EVAL board */ STM_EVAL_LEDInit(LED3); STM_EVAL_LEDOn(LED3); } if(!CAN_Init( CAN2, &CAN_InitStructure))while(1);}static void CAN_FilterConfiguration(void) { CAN_FilterInitTypeDef CAN_FilterInitStructure; /* CAN2 filter configuration */ CAN_FilterInitStructure.CAN_FilterNumber = 0; // Filter number = 0 (0<=x<=13) CAN_FilterInitStructure.CAN_FilterMode = CAN_FilterMode_IdMask; // Filter mode = identifier mask based filtering CAN_FilterInitStructure.CAN_FilterScale = CAN_FilterScale_16bit; CAN_FilterInitStructure.CAN_FilterIdHigh = 0x0300 << 5; //0x0000; CAN_FilterInitStructure.CAN_FilterIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterMaskIdHigh = 0x03FF << 5; CAN_FilterInitStructure.CAN_FilterMaskIdLow = 0x0000; CAN_FilterInitStructure.CAN_FilterFIFOAssignment = CAN_FIFO0; // FIFO = 0 CAN_FilterInitStructure.CAN_FilterActivation = ENABLE; CAN_FilterInit(&CAN_FilterInitStructure);}static void CAN_TxMessage(void) { CanTxMsg TxMessage; /* CAN message to send */ TxMessage.StdId = 0x321; TxMessage.ExtId = 0x01; TxMessage.RTR = CAN_RTR_DATA; TxMessage.IDE = CAN_ID_STD; TxMessage.DLC = 8; TxMessage.Data[0] = 0x04; TxMessage.Data[1] = 0x01; TxMessage.Data[2] = 0x00; TxMessage.Data[3] = 0x00; TxMessage.Data[4] = 0x00; TxMessage.Data[5] = 0x00; TxMessage.Data[6] = 0x00; TxMessage.Data[7] = 0x00; //while (1) { CAN_Transmit(CAN2, &TxMessage); //CAN_TransmitStatus(CAN2, 0); if(CAN_TransmitStatus(CAN2, 0) == CAN_TxStatus_Ok ) { STM_EVAL_LEDInit(LED4); // Initialize and STM_EVAL_LEDOn(LED4); // turn ON green LED if transmit was successful } //}}2016-03-09 04:33 AM
2016-03-09 04:46 AM
Yes I use a CAN MATE which will receive CAN message and monitor it in PC using CAN MATE pc application
2016-03-09 05:59 AM
Hi,
do you useany termination
resistor ? Please check also listen only mode
of CAN MATE, if it is possible for this adapter. Petr2016-03-09 06:00 AM
2016-03-09 07:01 AM
> Yes I use a CAN MATE which will receive CAN message and monitor it in PC using CAN MATE pc application
If this is just a passive listener, IMHO it won't help you much. Like clive suggested, you can try direct loopback.
2016-03-09 08:45 PM