cancel
Showing results for 
Search instead for 
Did you mean: 

My first STM32 based circuit, is this circuit ok?

terry23
Associate
Posted on March 18, 2016 at 14:48

Hi,

This is my first time working away from Arduino.

I am creating a simple CAN bus analyser using a STM32F105RBT6

I have used parts of circuits from various evaluation boards. 

But I am mainly concerned about the Power circuit. I want to be able to power from VIN or USB. Both are to be able to be powered at the same time.

I have also seen similar circuits using a 8mhz or 25mhz so I am not sure which to use.

The Image dialog on here doesn't seem to work on Safari or Chrome on Mac so please check out this post:

http://electronics.stackexchange.com/questions/215097/is-this-stm32f-based-can-bus-circuit-ok

#can-bus #stm32f105rbt6 #!stm32
1 REPLY 1
Amel NASRI
ST Employee
Posted on March 28, 2016 at 19:00

Hi gould.terry,

If you still need some help to implement your STM32F105 based board, I recommend you to refer to AN2586: Getting started with STM32F10xxx hardware development.

You find there more tips on how to design your hardware taking into accounts device characteristics.

-Mayla-

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.