cancel
Showing results for 
Search instead for 
Did you mean: 

How to download audio and video files to the STM32F746G-DISCO

smart-mir
Associate
Posted on March 24, 2016 at 13:50

ST wrote in ReadMe:

In order to program the demonstration you must do the following:

1- Open STM32 ST-Link Utility V3.7, click on ''External Loader'' from the bar menu then check 

   ''N25Q128A_STM32F746G-DISCO'' box 

2- Connect the STM32746G-DISCOVERY board to PC with USB cable through CN14

3- Use ''STM32CubeDemo_STM32746G-DISCO_V1.1.0.hex'' file provided under “Binary�? with STM32 ST-Link Utility

   to program both internal Flash and external QSPI memory

4- copy the audio and video files provided under ''Utilities/Media/'' in the USB key

5- Plug a USB micro A-Male to A-Female cable on CN12 connector

-> The internal Flash and the external QSPI are now programmed and the demonstration is shown on the board.

How could 4th point be done? There is only 1 Mb flash and no way to simply copy on disk.

And what about CN12 connect? What is it for?

2 REPLIES 2
Posted on March 24, 2016 at 23:48

Translation:

You put the files on a USB Flash Drive, that *you* supply, and you plug it into the DISCO board's USB HS port (CN12) with an adapter cable that you also supply.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Posted on March 24, 2016 at 23:54

http://www.amazon.com/Adapter-Samusung-Android-Windows-Function/dp/B00LN3LQKQ/ref=sr_1_1?ie=UTF8&qid=1458859786&sr=8-1&keywords=USB+micro+A-Male+to+A-Female

The N25Q128A is a 16MB (128Mb) device

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..