cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F103C8 - IAR throws error while downloading code with ST-Link

loder
Associate II
Posted on July 26, 2016 at 16:22

Hi,

i get these errors while downloading my code via the ST-Link (latest firmware) to my controller (STM32F103C8):


Tue Jul 26, 2016 16:22:30: IAR Embedded Workbench 7.1 (armproc.dll) 

Tue Jul 26, 2016 16:22:30: Loaded macro file: D:\Programme\IARWorkbench_STM32\arm\config\debugger\ST\STM32F1xx_XL.dmac 

Tue Jul 26, 2016 16:22:30: Loaded macro file: D:\Programme\IARWorkbench_STM32\arm\config\flashloader\ST\FlashSTM32F10xxx.mac 

Tue Jul 26, 2016 16:22:33: Connected to ST-Link/V2 [SWD mode 50 kHz] Firmware V2.JS6 (Probe no: 28611187) 

Tue Jul 26, 2016 16:22:33: Software reset was performed 

Tue Jul 26, 2016 16:22:33: Initial reset was performed 

Tue Jul 26, 2016 16:22:35: Warning: Write failed (CPU data abort) at Memory address 0x1FFFF800 

Tue Jul 26, 2016 16:22:35: Reset FLASH readout protection 

Tue Jul 26, 2016 16:22:35: Hardware reset with strategy 2 was performed 

Tue Jul 26, 2016 16:22:35: 736 bytes downloaded (2.42 Kbytes/sec) 

Tue Jul 26, 2016 16:22:35: Loaded debugee: D:\Programme\IARWorkbench_STM32\arm\config\flashloader\ST\FlashSTM32F10xxxRAM10K.out 

Tue Jul 26, 2016 16:22:35: Target reset 

Tue Jul 26, 2016 16:22:37: Unloaded macro file: D:\Programme\IARWorkbench_STM32\arm\config\flashloader\ST\FlashSTM32F10xxx.mac 

Tue Jul 26, 2016 16:22:37: The flash loader program reported an error. 

Tue Jul 26, 2016 16:22:38: IAR Embedded Workbench 7.1 (armproc.dll) 

Any ideas, what causes the errors?
2 REPLIES 2
Posted on July 26, 2016 at 18:23

What does IAR support have to say?

Why would it need to play with RDP or options bytes?

Is this a custom board?

Do you have similar errors with NUCLEO or DISCO boards?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
loder
Associate II
Posted on July 26, 2016 at 19:26

Thanks for your answer,

i didn't contact IAR because i don't know if it is maybe my fault.

It is the STM32F103C8 Board from China: https://i.ytimg.com/vi/DCjhJCk_bIE/maxresdefault.jpg

I don't have any other stm32 board so i can't test if it would work with the nucleo :(