cancel
Showing results for 
Search instead for 
Did you mean: 

USB communication at 50Mbps using STM32

udilevy
Associate II
Posted on December 13, 2016 at 09:18

Hi all,

I would like to implement USB communication at 50Mbps using STM32 as a device- based on ST's existing example code.

I would like to understand if this is possible to achieve using the standard example code assuming I will use the USB HS of the controller.

Can I use the CDC or MSC class code examples to achieve this?

#usb-bulk #usb-cdc #usb-otg #usb
0 REPLIES 0