cancel
Showing results for 
Search instead for 
Did you mean: 

VREFINT, Temperature sensor always returns 4095 value (STM32F3 Discovery board)

bhcuong2008
Associate II
Posted on May 01, 2016 at 21:43

The original post was too long to process during our migration. Please click on the attachment to read the original post.
2 REPLIES 2
bhcuong2008
Associate II
Posted on May 02, 2016 at 09:23

When I disable bit VREFEN, value of VREFINT is still 4095.

bhcuong2008
Associate II
Posted on May 02, 2016 at 11:22

Just for more information. I also tested with VBAT, and the return value is about 3050. On the board, VBAT is connected to VDD = VDDA = VREF+. If correctly, it must be 4095.

Testing with other external channels (ADC1_IN2/IN3), the result is ok.

So, what's the problem with internal channels? I can't figure out it.