2016-06-10 08:23 AM
The purpose of this post is to save other developers the time I have spent tracking this down. Bear with me on this - its messy.
Line 1108, of stm32f1xx_hal_rcc.c isif (pllmul == aPLLMULFactorTable[(uint32_t)(RCC_CFGR_PLLMULL6_5) >> POSITION_VAL(RCC_CFGR_PLLMULL)])
You'll need to know that&sharpdefine RCC_CFGR_PLLMULL6_5 ((uint32_t)0x00340000)
&sharpdefine RCC_CFGR_PLLMULL ((uint32_t)0x003C0000) andconst uint8_t aPLLMULFactorTable[12] = {0, 0, 4, 5, 6, 7, 8, 9, 0, 0, 0, 13};
You'll find that(RCC_CFGR_PLLMULL6_5) >> POSITION_VAL(RCC_CFGR_PLLMULL)
is a constant that evaluates to 13. And when this is used to indexaPLLMULFactorTable
[12], it generates an array bounds overflow. This would seem to be a bug in the HAL library (though please tell me if I have got this wrong). I encountered this in trying to understand why I was occasionally getting the wrong baudrate. Scary, eh? #hal-bug2016-06-11 01:23 AM
The problem would appear to be in the lookup tables in stm32f1xx_hal_rcc.c (and stm32f1xx_hal_rcc_ex.c). [I can see now that I should have mentioned that this issue was found on STM32F105 as I think that makes a difference.]
I read from 13902.pdf: 8.3.2 Clock configuration register (RCC_CFGR)Bits 21:18 PLLMUL[3:0] : PLL multiplication factor
1101: PLL input clock x 6.5 So it would appear that the index of 13 is correct but that the table is not. I think
const uint8_t aPLLMULFactorTable[12] = {0, 0, 4, 5, 6, 7, 8, 9, 0, 0, 0, 13};
should have beenconst uint8_t aPLLMULFactorTable[14] = {0, 0, 4, 5, 6, 7, 8, 9, 0, 0, 0, 0, 0, 13};
Hopefully ST will fix this issue in future versions of the HAL source code.2016-06-13 05:10 AM
Hi richard,
Thank you for the feedback. We will check this internally. -Hannibal-2016-06-14 01:43 AM
Hi Hannibal,
Thanks for taking a look at this. Also, I should apologise for posting in ''STM32'' when perhaps it should have been issue posted in ''STM32 Software Tools and Firmware
''. While we are in this area, can you explain why these lookup tables appear to be located in RAM?. Wait...I'd better start this as a new discussion in ''STM32 Software Tools and Firmware
''. Watch that space 😉 Thanks, Richard2016-06-15 05:57 AM
Hi Richard,
This is not directly related to the subject, but I'd like to know where do you find this file? I use mbed but I can't go far in programming with it. The examples I have are short, clear and all, but I can't find out how to modify them efficiently, and so I wanted to see if the answer could be in the default libraries (.h + .c/.cpp ). When I export an mbed project into Keil, I can see many many .h, like the one you mention in this post, but not the .c related to them. So my question is: where are they?2016-06-16 02:26 AM
Antoine.PM, I'm sorry but I don't know anything about mbed.
>where do you find this file?stm32f1xx_hal_rcc.c
is part of the stm32cubef1 library provided by ST and available at their website. This file typically unpacks to ...\Drivers\STM32F1xx_HAL_Driver\Src >This is not directly related to the subject Its probably better if we don't piggyback one discussion on the back of another. Better to start a new discussion with a relevant subject so that other developers can easily find any useful information that is posted.2016-06-16 03:52 AM
Ok, thank you for your answer, I'll keep digging then :p
You're right about the multiple questions on the same subject, of course, but I have several little questions about different aspects of coding on stm32 and using related softwares, and I thought it was better to ask them directly than to flood the forum with my newbie and sometimes confused questions :\