2016-08-02 05:43 AM
I use two ADCs, working together on two different signals.
These two signals have the same frequency and amplitude. They are shifted, Signal 2 has a phase of 90°.The DMA put the converted values in an array. This array is printed circularly in the Debug Viewer.I have one column of values for each signal.The ADCs seem to work correctly, however I have a doubt: is it possible that the Trace is too slow?Typically, I have this kind of result: </colgroup>1986 5
1924 3
1865 3
1803 4
1742 5
1683 11
1623 18
1564 27
1503 34
1439 50
1376 54
1314 68
1260 88
1202 108
1145 131
1091 155
1035 179
979 208
929 239
884 280
834 314
784 347
733 385
687 423
641 463
593 501
554 546
510 589
470 635
423 681
392 3603
2556 3578
2611 3553
2667 3524
So you can see here that there is a gap, several values are likely skipped during the printing process.Here is the graphic output of the values from both ADCs.As you can see, this happens several times, but this left aside, the two signals are correctly treated.During the execution in debug mode, I have the message ''Trace: data overflow''.So I think it is just about the display of the values, but I wanted to be sure.Should I be concerned about this, or should I just assume that the values exist in the memory and the Trace just fails to show them properly?2016-08-02 06:21 AM
> The ADCs seem to work correctly, however I have a doubt: is it possible that the Trace is too slow?
If your trace runs concurrently with debugging over SWD, sure. Debug and trace are sharing bandwidth in this case. Professional debug pods with real-time trace (ETM) will cost you about 1k bucks (€ or $). Consider tracing (in your case) just useful for verification. Once the code-under-test is proven to work, turn tracing off.
2016-08-02 06:23 AM
Good to know, thank you 🙂