cancel
Showing results for 
Search instead for 
Did you mean: 

LSM303AGR magnetometer SET/RESET procedure

marziano
Associate
Posted on August 23, 2016 at 15:29

Hi,

I'd like to perform a SET/RESET procedure on the LSM303AGR magnetometer. As explained in the AN4825 pag. 17, if the user performs a single read, the bit OFF_CANC in CFG_REG_B_M must be set to '1' to invert the impulse polarity between a single read and the next one. Has this bit to be set high before the two consecutive readings or between the first read and the second one?

#offset #reset #lsm303agr #set
0 REPLIES 0