cancel
Showing results for 
Search instead for 
Did you mean: 

FOC SDK with eclipse AC6

David Martins
Senior
Posted on November 09, 2016 at 16:41

Hello everyone.

Recently I started to create a project to make control of a BLDC engine.

I used, until now, the compiler eclipse AC6. I have read here, in the forum, that some people are using the SDK with AC6.

Can someone explain the procedure, please?

Thank you very much.

#ac6 #foc-sdk
2 REPLIES 2
Sirma Siang
ST Employee
Posted on January 10, 2017 at 09:53

Hello

Martins.David

,

You can refer to openSTM32 website.

Following link details how to install eclipse plugins to be able to compile CubeMX generated code:

http://www.openstmorg/Installing+System+Workbench+for+STM32+from+Eclipse?structure=Documentation

hope it answer your question.

If I missunderstood it, could you please elaborate a bit what you are trying to achive ?

Thanks in advance.

KR

Sirma

Laurent Ca...
Lead II

The question has been moved from the "Motor Control Hardware" section to the "STM32 Motor Control" section (the question is about the STM32 MC SDK). 

Best regards