cancel
Showing results for 
Search instead for 
Did you mean: 

Reset a STM32

guillaume215
Associate
Posted on June 22, 2016 at 18:45

Hello

I have a STM32F429I - DISC1 microcontrollers. After mishandling likely, the microcontroller was not started.

When I plug in the USB cable, my computer tells me that the device is not working properly. The only LEDs that are turned on are:

- G2 ((red) for 3.3 V power-on)

- LD6 ((RED) OC  (over- current))

Is it possible to reset the microcontroller or reboot?

Thank you

 

1 REPLY 1
Posted on June 22, 2016 at 18:59

Physical damage is not something you can fix with a button.

If you have loaded some broken software you can strap BOOT(0) to VDD and have the device boot into the system Loader, from where you can erase the errant code.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..