cancel
Showing results for 
Search instead for 
Did you mean: 

UART CTS/RTS HAL based example code for STM32F4xx device.

pradeepsysargus
Associate II
Posted on February 04, 2017 at 13:06

I am trying make communication between RN4020 Bluetooth module and STM32F411RCT MCU.

They are connected with UART and CTS/RTS, hardware flow control is recommended for this communication.

It would be great if I could get some examples to proceed.

Thanks,

#uart-hal #stm32-uart-hardware-flow-rts/cts #stm32f4
1 REPLY 1
Rejane Durand
Associate II
Posted on March 07, 2017 at 16:01

The original post was too long to process during our migration. Please click on the provided URL to read the original post. https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I6n6&d=%2Fa%2F0X0000000bvX%2F7A7rmpTYL2plvvD7eyloh341EKi_U5pFl4Z8vYIjpgE&asPdf=false