cancel
Showing results for 
Search instead for 
Did you mean: 

IpWayStudio Eclipse IDE. TCP/IP and touch screen applications on STM32 Discoveries

ingdm
Associate

Posted on July 12, 2016 at 11:20

Dear users,

I have developed the IpWayStudio IDE based on Eclipse. You can get it here: /external-link.jspa?url=https%3A%2F%2Fsourceforge.net%2Fprojects%2Fipway%2F

.

You can find some demo applications inside. All you need to do is:

- downalod IpWayStudio from here: 

/external-link.jspa?url=https%3A%2F%2Fsourceforge.net%2Fprojects%2Fipway%2F

- get a discovery board among the following: 32F746GDISCOVERY, 32F769IDISCOVERY or NUCLEO-H743ZI .

- runni ng your application.

You will find a Quick Start Guide about IpWayStudio and an application note of the demos.

The demos are based on IpWay/HOST free Tcp/Ip Stack Library, moreover they make also use of other software component as touch screen library and so on.

The project is frequently updated, stay tuned!

Enjoy it!!!

Best Regards.

1 REPLY 1
Nesrine M_O
Lead II
Posted on July 13, 2016 at 15:02

Hi di_martino.giovanni,

Thank you for sharing your application with us.Hope that this will be helpful for forum users.

-Syrine-