cancel
Showing results for 
Search instead for 
Did you mean: 

What is length of Evt_Blue_Gatt_Procedure_Timeout?

rdscliff
Associate II
Posted on August 16, 2016 at 03:37

Using BlueNRG 6.4b, I received an event that I think is Evt_Blue_Gatt_Procedure_Timeout (FF 05 02 0C 01 08 00).  Document UM1755 says there should be 2 bytes after the event code but I'm seeing 3 on my SPI analyzer.  Am I interpreting the event correctly?

1 REPLY 1
mehdi
Associate II
Posted on January 10, 2017 at 16:04

Hi,

i'm using the BlueNRG with the firmware 6.4 with a smartphone application that send indications to the blueNRG (Slave), and after a delay, the BlueNRG send this event to my embedded application ... do you have an idea on why this event is generated ? in the documentation they say 'This event is generated by the client/server to the application on a GATT timeout (30 seconds).' but 30 seconds before, nothing happens, the BlueNRG is receiving indications and it acknowledges every indication received.

Thanks,

Mehdi