cancel
Showing results for 
Search instead for 
Did you mean: 

LPS25HB: Pressure resolution config. and One shot mode

bvn123
Associate II
Posted on October 03, 2016 at 18:03

Hi,

in datasheet for LPS25HB ('DocID027112 Rev 3'), page 27, the register

'RES_CONF (10h) Pressure and temperature resolution'

is described.

Question1: Is the 'Nr. internal average' (table 18) applicable for One-shot mode?

Q2: If it is so, would be selected Nr.internal average influence on conversion time for One-shot mode at all?

Q3: How long would be conversion time in One-shot mode?

If there is concerned above influence (see Q2), what is the conversion time, when Nr.internal average=8 and when

Nr.internal average=512?

Best regards.

#lps25hb #pressure-sensor
0 REPLIES 0