cancel
Showing results for 
Search instead for 
Did you mean: 

Information on patch.xml workflow

robertabel9
Associate
Posted on November 18, 2016 at 17:38

I'm currently using SPC5Studio 4.2.1 (4.2.1.201607051420) and use it to develop on an SPC560B-DIS evaluation board. I noticed that edits I make to component files in the lib sub-directory are handily stored in regular diff format in patch.xml.

However, I would also like to edit files in e.g. the cfg sub-directory, so I manually created the following entry inside the patch.xml file:

<?
xml
version
=
''1.0''
encoding
=
''UTF-8''
?>
<
SPC5-Patch
version
=
''1.0.0''
>
<!--It is your patch repository, do not break your XML File.-->
<
files
>
<
file
componentId
=
''org.chibios.spc5.components.spc5hal''
version
=
''1.0.0.201607011046''
path
=
''component/cfg/halconf.h''
user
=
''false''
>
<
diff
>
<![CDATA[--- components/portable_spc5_hal_component/cfg/halconf.h
+++ components/portable_spc5_hal_component/cfg/halconf.h
@@ -79,7 +79,7 @@
* @brief Enables the I2C subsystem.
*/
#if !defined(HAL_USE_I2C) || defined(__DOXYGEN__)
-#define HAL_USE_I2C FALSE
+#define HAL_USE_I2C TRUE
#endif
/**]]>
</
diff
>
</
file
>
</
files
>
</
SPC5-Patch
>

However, these manually introduced patches aren't being applied once I recreate the component tree. Is there some setting/trick/... to enable this? Is my syntax wrong? Or is it plain not possible to patch files outside of the lib sub-directories at the moment? #spc5studio-patch
3 REPLIES 3
Erwan YVIN
ST Employee
Posted on November 21, 2016 at 09:57

Hello robert ,

You can not patch a configuration file (cfg directory).

cfg file is a file generated from the GUI.

I2C driver does not exist on B Discovery (HAL & RLA)

HAL Side : i2c_lld.c should be created

RLA Side : i2c_lld.c should be created

we have a change request to create I2C for B Discovery

(i am writing a private email for you)

Best regards

Erwan

robertabel9
Associate
Posted on November 22, 2016 at 14:31

Hi Erwan,

It's unfortunate that the cfg files cannot be patched. The reason I'm asking is that I implemented my own i2c lld interrupt-driven driver but use the ChibiOS hal to be compatible. So far I haven't received your private e-mail.

Regards,

Robert
Posted on January 18, 2017 at 16:49

Hello Robert ,

You should check the post

https://community.st.com/0D50X00009XkYQQSA3

Best regards

Erwan