cancel
Showing results for 
Search instead for 
Did you mean: 

Run Nucleo only with power, no PC USB connection

harald
Associate III
Posted on September 01, 2016 at 18:33

Hy,

I start to work with the Nucleo Platform. I have several Nucleos and can program them with System Workbench for STM32, no problem. But when I connect the USB cable to either a USB power pack or a PC that has not installed the ST-Link drivers, my program in flash won't run.

Device is obviously powered, the red LED LD1 flashes slowly, but my program won't start.

As soon as I connect the board to a PC with the ST-Link driver installed, my program starts running again, so obviously it is still in flash.

Is this the expected behaviour? Is there anything I can do about this? I wanted to use the system for a technical demonstration but am not able to connect it to the development PC all the time.

Best regards

Harald

#nucleo #usb-power
2 REPLIES 2
Posted on September 01, 2016 at 20:48

This sounds like an issue that was seen with older ST-LINK firmwares used on NUCLEO and DISCO boards, get the current ST-LINK Utilities, and have it update the ST-LINKs you are using.

Tips, buy me a coffee, or three.. PayPal Venmo Up vote any posts that you find helpful, it shows what's working..
harald
Associate III
Posted on September 02, 2016 at 01:03

Hy,

that was it!

0690X00000605bfQAA.png

Works perfectly now...

Thanks and best regards

Harald