cancel
Showing results for 
Search instead for 
Did you mean: 

Where is the Graphics Library in ST32M CubeMX ?

roythomas
Associate II
Posted on August 21, 2016 at 14:34

I m New to STM32 and TFT.

I need to Interface a TFT LCD with Touch screen to ST32103CB MCU.

Which is the library or example project ST Micro provides for this task for me to begin as a template.

The example I found is using for High Density devices.

Please suggest where I should start Looking

#stm32 #lcd #tft #graphics
1 REPLY 1
Posted on August 21, 2016 at 16:28

Does your chosen device support the FSMC bus, is there a reason the example is only viable on the High Density device?

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..