cancel
Showing results for 
Search instead for 
Did you mean: 

How to connect ST Link V2 Debugger to STM32F&46NG Discovery board

vasukisoni
Associate
Posted on September 07, 2016 at 12:33

What are the pin connection to be done or any other connectors or shield we need to use to connect St Link V2 Debugger to STM32F746NG. I have this doubt because older boards like STM32F4 have JTAG socket in the board to connect to the debugger but in STM32F746NG Discovery board, there is no JTAG. Only USB Connector is there but ST Link V2 debugger doesn't have any connector to connect to the board via USB.

Please support me with this query.

Thanks

#stm32 #stm32f4 #stlink #st-link #stm32f746-disco
1 REPLY 1
Posted on September 07, 2016 at 15:03

What's the point in doing this vs using the ST-LINK built onto the board?

You'd want to connect 3V3, GND, SWDIO, SWCLK, SWO and NRST to get an SWD connection, not sure if enough pins are exposed to get JTAG functionality.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..